Hi,
For continuous balancing operation ,I send start balancing (0x10 OR 0x30) followed by stop balancing (0x00):
When I send 0x10 then the return code is 0xA1,When I send 0x00 then the return code is 0xa0,and the emb1428 and emb1499 are work well.
But,when I send 0x30 then the return code is 0xA3,when I send 0x00 then the return code is 0x20 or 0x60, the emb 1428 works well but the emb1499 doesn't.
I don't understand under the two conditions ,the emb1428 part work well (Vplus-Vminus = one single cell's voltage),the emb1499 part is same why the second condition isn't work?