Hi,
Our customer uses BQ7790502 to protect Li battery, and it can protect battery when SCD, OCD, OTD, OTC, OV or UV occur. The problem is that when fault occurs and the battery is protected, the fault recovers automatically after about 2 ms. Bucause the fault recovery method of BQ7790502 is load removal, so the fault should recover when the load is removed, rather than it recovers automatically.
They tested TI EVM with BQ7790500, on which the fault recover through load removal + delay, and it can keep protection state, and not recover automatically. Then they used BQ7790502 instead of BQ7790500 on TI EVM, however, the fault can also recover automatically. So why BQ7790500 can keep protection state, but BQ7790502 can not keep protection state and recover automatically when fault occurs? I am waiting your reply, thanks!
Note: the screenshot of datasheet of BQ77905 and the customer's schematic as follows.