Hi,
We are using BQ76PL455AEVM for developing our BMS.
We are using EVM GUI. These are our observations
1.We tried to balance our cells( note that charger was not connected) and after 2 hours of balancing, the total voltage reduction was 5mV, balance current was 50mA.
2.There was an offset in the adjacent cells while balancing. We were balancing cell2, so the offsets were +10mV in cell1, -40mV in cell2 and +30mV in cell3.
Following are our doubts:
1. Can we balance the cell at any time or do we need to connect the charger to balance?
2. Can we balance at any voltage and at any voltage difference?
3.Is the time for balancing is expected like in our observation?