I am trying to implement the BQ76920 in a battery monitoring application. The schematic is below
When reading the individual cell voltages I have found the VC2 is very inaccurate, usually around 3.67V when it should be around 4.14V.
Actual reading (V) | BQ76920 Reading (V) | |
Cell 1 | 4.13 | 4.13 |
Cell 2 | 4.14 | 3.62 |
Cell 3 | 4.08 | 4.67 |
Cell 4 | 4.14 | 4.13 |
Total | 16.4 | 16.53 |
As you can see from the above table there is quite a discrepancy between my readings and the actual ones. What could be causing this inaccuracy and how can I rectify it?
Many thanks,
Tom