Other Parts Discussed in Thread: BQ40Z50,
I would like to combine two 3s2p Li-ion packs to make one 3s4p pack. Each of the 3s2p packs utilize the BQ2947 for over-voltage protection and both use the BQ40Z50 to balance cells. If I start with two fully charged cells they may slowly drift apart from each other. However, it seems if one pack is above the other, it will try to charge the other and trigger the over-charge/over-discharge current protection. It doesn't seem like good practice to anticipate a case where the protection be tripped, but it seems that the part is designed to handle the potential mismatch until they are brought back into synch.