Dear TI,
i'm Valerio.I have application with BQ76940,BMS maangement in litium cell.
I try to simulate internal chip fault indicator in demo board with short across to C2 or C3 cap.
i have to simulate internal fault in i2c receive flags :
DEVICE_XREADY (Bit 5): Internal chip fault indicator. When this bit is set to 1, it should be cleared by
the host. May be set due to excessive system transients. This bit may only be cleared (and not set) by
the host.
0 = Device is OK.
1 = Internal chip fault detected, recommend that host microcontroller clear this bit after waiting a
few seconds. Remains latched high until cleared by the host.
I don't view in comunication I2C this bit don't go to 1,how to in demoboard for set to 1 this bit flga?
Thanks
Best Regards
Vale