This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

BQ25890: EMI mitigation

Part Number: BQ25890

HI, 

I'm using the bq25890 in my design to charger a 7200mAh battery. In charge mode, my device is failing radiated emission test, and the source of the emission ihas been narrowedd down to the charger IC. Unfortunately this IC does not give enough flexibility to play with the settings (like gate driver slew rate control, etc) 

  • Are there equivalent IC's that have better EMI response that TI carries
  • Are there any suggestions to help reduce the noise level

I'm charging at a rate of 3.5A using a quick charger IC that provides a 11.5V @ 1.5A.  

The device is charging through USB via a wall wart charger (quick charge)

Thanks

  • Guru 59275 points

    As with all buck converters, input capacitor placement is critical to lower EMI.  Placing C172 as close as possible between PMID and GND and/or adding a small decoupling capacitor (0.01uF to 0.1uF) usually mitigates EMI.  If not, then adding a properly sized RC snubber from SW to GND will mitigate EMI at the expense of efficiency.  Attached is a document the further explains these recommendations.bq2589xbq2419x_29xlayoutandEMIrecommendation.pdf

     

  • In reply to Jeff F:

    Jeff,
    Thank you for your reply. I'll give some of these a try and i'll let you know if i have further questions.
  • In reply to Jeff F:

    Hi Jeff

    I have some questions about some the app note as well as my system response. I notice something strange happenning on the switch node. SW_OUT (on my schematic). There is no visible ringing (no overshoot on the rising edge) but there is ~1V undershoot on the falling edge. The strange thing is that the undershoot is held low for some time before recovering, but then right before the start of the rising edge it drops again by approximately the same voltage. The question is why is it behaving like that. I have never seen this. Could this have anything to do with Low side power FET parasitic capacitance ? 

    YEL: input current

    RED: SW_OUT

    I also see some high frequency switching on my input voltage that decoupling capacitors do not seem to remove. I placed a 1nF cap across the 1uF cap on VBUS. The oscillation frequency of that high switching noise is ~230MHz. Do you normally recommend using an LC filter to keep that noise from migrating to the USB charging cable and radiate or you have a different take on it. 

    YEL: input current

    RED: VBUS voltage

     

    My last question is out of curiosity: 

    How is the switcher being regulated? I don't see on the block diagram on page19 of the datasheet where the error signal is being sensed and how the control loop operates.

    Thanks again for you help. 

  • Guru 59275 points

    In reply to user4300350:

    Your charger is oscillating. I have reviewed the schematic again and don't see any obvious issues. If you remove or short FB12, does the oscillation go away? If you add additional capacitance at SYS or at PMID, does the oscillation go away? If not, can you send your layout and I will review.

    Regarding the feedback error signal, the SYS and BAT pins are the feedback points. There are error amps in the middle left with SYS and BAT points. The control method is a combination of voltage mode and current mode control.

     

  • In reply to Jeff F:

    Yes, i forgot to mention the oscillation in my previous poIt because i was able to mitigate that with a 10uF on PMID (see screenshot below) I also got similar results adding the same capacitance to VBUS. That being said, from a USB compliance prospective the added capacitance can be an issue (higher inrush current upon insertion of USB, etc) but between VBUS and PMID where do you recommend placing this additional capacitance to lower this oscillation.

    How to do prefer i send you the layout. A 2D screenshot may not give you a good idea of placement. 

    BOTTOM and power plane with copper pour for VBUS 

    TOP


  • In reply to user4300350:

    Jeff,
    I still haven't gotten an answer about the behavior my switching node is seeing (described in May 19 post), Any thoughts on what's going on there ?or the idea about the LC filter on the input as a way to reduce our switching noise. 

    Also what about the idea of adding an LC filter on the input as a way to reduce our switching noise. What type of care should I take to ensure my LC filter doesn't affect the switcher stability. What's the input impedance at VBUS ?

    Thanks

  • Guru 59275 points

    In reply to user4300350:

    I have never seen this charger oscillate in my 3 years of supporting of it.  Can you send the register settings when you see this oscillation?    In the past with other chargers, adding an LC on the front end usually caused oscillations.  Like any buck converter, the input impedance at VBUS is negative resistance.  I will ask if design has characterized it.

     

  • Guru 59275 points

    In reply to Jeff F:

    Is register 13 bit 7 reporting that you are in VINDPM? If so, if you change your input voltage or change the VINDPM using the Force VINDPM bit (register 0D bit 7) and then changing the value (register 0D bits 0:6), does the oscillation go away?

    Regarding your layout, the single via for PMID from top to bottom is adding a lot of resistance and inductance. That capacitor is the input to the buck converter and so sees large current spikes.

     

  • In reply to Jeff F:

    Hi Jeff,

    I gave some thoughts to the scope shots I shared with you that showed an apparent "oscillation" of the VBUS line, and input current. Something I forgot to mention in case you have not noticed is the fact that the voltage waveform is AC coupled. The current waveform looks more as if the switcher is in continuous conduction mode and the voltage waveform is more of the

    The current waveform (YEL) looks more as if the switcher is in CCM with quite some capacit

    The voltage waveform (RED) looks more as if it's more of a ripple due to the amount of impedance (charger output impedance) on that path.

    Any additional feedback on the layout woujld be really appreciated.

    Thanks
  • In reply to user4300350:

    In our current layout, the analog and digital ground are not separated. We are connecting all pins to our system ground. I know the datasheet example block diagram show separate grounds. I'd like to know whether that's necessary?

    Thanks

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.