This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

BQ25703A: Battery charging Using EV2300

Part Number: BQ25703A

Hello E2E Community,

For POC, we are testing with BQ25703A EVM & EV2300 kit. I am using the Battery Management Studio (bqStudio) Software Suite v1.3.54.1 - Build 1.

I am not able to see the recommended target  mentioned in BQ25703A EVM i.e., “Charger_1_00-bq25703AI2C.bqz” in the list of supported targets by tool.

So does EV2300 support the BQ25703A EVM for enabling the battery charging configuration ? If yes, then please provide the steps to do so.

Can i select some other charger target which may be compatible in configuring battery enable ?

If not then does it need EV2400 kit for this ?

Also am i using the correct version of the tool i.e., bqStudio Software Suite v1.3.54.1 - Build 1 ?

Regards

Devendra Singh Solanki

  • Devendra Singh Solanki,

    Please copy the attached bqz file to bqstudio's config folder.

    2438.Charger_1_00-bq25703A.bqz

    If the EV2300 can support bqstudio, you can try the attached Charger_1_00-bq25703A.bqz file.

    Best Regards,

    Wang Li

    Battery Charger Solutions

  • In reply to Wang5577:

    Dear Wang5577,

    As per your instruction i copied the 2438.Charger_1_00-bq25703A.bqz file to bqstudio's config folder.

    But it still did not show in the list of supported targets. So i renamed the config file to "Charger_1_00-bq25703AI2C.bqz".

    Now it shows the BQ25703A as one of the supported targets. So now i move to next steps of changing “update mode” from “immediate” to “manual”. Upto this step it is done successfully.

    Now when i click on “Read Register” it shows me a "Device ACK Error". Attaching the screenshot of the same. 

    Please help to resolve this issue.

    Regards

    Devendra Singh Solanki

  • In reply to Devendra Singh Solanki16:

    Devendra Singh Solanki,

    Please change "Tgt address" from "D4(6A)" to "D6(6B)".

    If it still has trouble, please send me the SDA and SCL waveform.

    Best Regards,

    Wang Li

    Battery Charger Solutions

  • In reply to Wang5577:

    Dear Wang Li,

    After changing the target address from "D4(6A)" to "D6(6B)", i clicked on “Read Register” it still shows me "Device ACK Error".

    I probed the SDA & SCL signals as per your suggestion,but they are at Logic High (i.e., 3.3V) for the whole duration while i select the target charger, change the target address & click on read register. Neither SCL nor SDA signal goes low.

    I tried using the Version 1.3.80 of BQStudio as well with same steps of copying new config file & changing target address. This also shows me the same "Device ACK Error".

    Is it possible that it needs EV2400 to configure the BQ25703A EVM. EV2300 cannot be used for this.

    Let me know your input on this.

    Regards
    Devendra Singh Solanki
  • In reply to Devendra Singh Solanki16:

    Devendra Singh Solanki,

    It is possible that computer OS needs EV2400 to configure the BQ25703A EVM. EV2300 may not be used for this computer.
    EV2300 may need to install the unofficial drivers for windows 64 bit. There is a forum post about this.

    Best Regards,

    Wang Li

    Battery Charger Solutions

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.