I'm in search of a product (or set of products) that will take 5V over USB and provide power to my system at a regulated 3.3V, and also manage the charging/discharging of a 3.7V LiPo cell.
I would like a variable current draw so that the device is USB spec compliant, but will also draw as much power as available from a wall wort to both supply the system and charge the battery. If the IC could handle determining the amount of permissible power draw from the USB data lines, that would be idea.
An output current of 1.5A or greater is required.
Thanks for any input, that combination of features is hard to search for!
- Brent