I have a 30 amp controller and a 250w schott solar panel on a camper well the controler goes into an error E2 which is high voltage checked voltage and there was 17.5 volts comeing from the solar panel and 16.1 going to the batteries, disconnect the solar the error goes away and the voltage from batteries is 13.5 volts . reconnect solar panel and the same thing happens. Anybody know what to do? Thanks Dean