Hi,
I am Aravind. I kindly need the battery charger solution for the below combination from TI for one of my customer.
the battery charger should have the ability to charge 4 numbers of 3.7V 830mAh Lithium-polymer batteries, 2 numbers of 14.8V 5080mAh Lithium-Ion batteries and one 11.1v 2200mAh Li-Poly battery. Additionally this device should support the use of two 5V USB ports for external devices (no USB communication, only for DC power 5VDC +/-5%, 0.5A)
Input voltage to the battery charger shall be 18VDC.
Kindly help me out.
Regards,
Aravind.