Recently I've ordered a BQ24650 EVM. From what I understood is at 17.8V input, the voltage at MPPSET is 1.2V and if it's less than 17.8V it goes to voltage regulation mode by reducing the charging current. The question is:
1. When input drops below 17.8V, the charging current drops to zero with a 12V Lead Acid battery connected (~12.3V), why?
2. A PV panel will give lesser voltage (say <13V) during morning and evening, so will it still charge a 12V Lead Acid battery?