Hi,
I read the documentation and quite qood understand the datasheet of BQ24210 and I researched all the topics about it in forum but one point is not clear on my side. Now my point is:
Considering working range of 3.5v - 7v, is the solar panel MPP should near below 7V ? In this case max. open circuit for a solar panel should be 8.75V (assuming 80% MPP). Am I right In this point?
If I am right then the selecting resistor for VPDM formulation is quite looks limited with range 1k-10k Ohm and in this case VBUS voltage should between 3.65V-5V. So how one can calculate for near below 7V?
Am I missing something or the chip actually setted up for VBUS 5V anyway? In this case max. possible voltage for a solar cell should be around 6V considering its MPP. Is this right?