Hi All,
I have one question, I'm using a solar cell to power a LiPo battery. This battery is giving power to a micro controller (MSP430) and to an additional circuit. At the moment when the battery is being discharged I have to recharge it using the solar cell -which is configured by the micro controller-. The issue is that I'm not sure if I can recharge the battery and give power to the micro controller at the same time. I could not disrupt the power because if I do that all the system would die. What can I do?
I google it but I did not see any credible source.