Dear Sir,
I have bq24163 charger in target desing and I have problem with output voltage on SYS rail. According to datasheet there should be 3.5V in default without battery. But there is voltage about 5V with 5.5V on input and 6V with 7V input. Also when 5V is applied to input then charger reports input adapter error and output is only pulsing (on recovery test).
I reviewed design according to reference desing and can't see any problem. Could you please give me some clue where can be problem?