This is regarding BQ24055 IC:
For processor or host monitoring, the processor’s power rail is 3.3V VCC. I need to monitor the CHG and PG pins. What values should I use for pull-up resistors? I need to monitor when the battery is fully charged, change in STATUS.
- Between the processor’s power rail and CHG pin?
- Between the processor’s power rail and PG pin?
I am using STM32L151VBT6 MCU.
I used 3.3K and 4.7K resistor values for pull-up; however I do not see change in STATUS. The charger CHG LED remains on and no change in STATUS on MCU display. This is on a fully charged battery.