I have a question about the current limit on bq24250.
According to Table 1, the ILIM can be set to 100 mA by EN2=1 and EN1=0. Does that mean that no external resistor is required on ILIM pin?
The same question arises when we set the ILIM by I2C. Do we still need a resistor for the ILIM pin? If not, then according to the table for pin description, which says "If an external resistor is not desired, short to GND for a 2A default setting", the ILIM would be 2A!
Thanks,