Hello,
we have a circuit, see attached image.
The power consumption is very low (10uA at 3,3V).
We have a Lipo, that will be charged from the bq24040. When the bq24040 is in the circuit, the power consumption is much to high (350uA). Then we put the bq24040 out of the circuit, the current was down to 10uA.
In the datasheet, there is only 1uA, that is going into the OUT pin.
Do you have any ideas, what could be the problem of that?
Best regards,
Johannes