Hi
I'm searching a solution to power a product from a serial port input @ 31kbps, serial port signal is a current loop of about 10mA.
My system power requirement is about 30mA @ 3V.
My idea is then to use a Li-Ion battery (about 200mAh), that could be charged from the serial port.
Serial signal could be from 2.5 to 5V when idle, going to zero while data are transmitted.
I plan to use the BQ25570, serial input connected to Vin, with a small input current of 10 to 20mA used to charge the single cell battery.
1) I do not find in the data sheet if the input charge current can be set as low as 10mA ?
2) If Vin is 5V with 20mA max, will the boost be auto-disabled ?
Any suggestion, comments are welcome
thanks