Hello,
Are there the device which doesn't have precharge function ?
Requirement is as below.
Requirement is as below.
Vin: 12V +/- 0.5V
Vout : 7.2V~10.5V
Iout(max): 1A
Switching tipe
CC/CV control
Best Regards,
Ryuji Asaka
Ryuji Asaka