This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24075 not working without battery

Other Parts Discussed in Thread: BQ24075

I'm using bq24075 with typical schematic from DS, SYSOFF, CE, EN1 tied to GND, EN2 to OUT.

47k on TMR, 750E on ILIM, 2.2k on ISET, 10k on TS. 4.4V on IN.

When battery is connected everything is ok, but when no battery connected and only external voltage on IN is applied, bq24075 is not started and no voltage is on OUT pin.

If I connect the battery, then connect external voltage, it starts, and I can disconnect the battery and the system is running. But It need to able to run without battery too.