Hi, I want to power a wireless sensor network (almost continuously),but am confused in purchase of bq25504 or bq25570 or bq25505,Can any one please help me to decide which is more suitable?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The boost charger core of each is essentially the same, with some of the specs having tighter tolerance on the bq25570 and bq25505. Also the bq25570 and bq25505 require fewer resistors because the VOC_SAMP pin can be tied to VSTOR or GND for fixed 80% solar panel MPP or 50% GND. In addition, the threshold for the integrated battery overdischarge prevention FET is fixed internally at 2.0V for these two devices where the bq25504 requires external resistors to set the threshold for this feature.
If you will have a primary, non-rechargeable battery as a back-up, then I suggest bq25505 which has gate driver for an external PFET based MUX to switch the system load between the primary and secondary rechargeable battery.
If you need a second power rail that is lower than the battery, then I suggest the bq25570 which has an integrated buck converter that can provide that rail.
Thanks for your suggestion.
Also is it possible to use bq25570EVM as bq25504EVM board by disabling buck converter,will both be exactly the same.
But is it possible for continuous operation of wireless load with this bq25570EVM board.
If you disable the buck on the bq25570 with its VOUT_EN pin, it will operate the same as the bq25504, except the VBAT_UV threshold is internally fixed at 2.1V. The bq25504 allows you to set the VBAT_UV threshold, to prevent battery overdischarge, with external resistors. If your battery has isn't own internal protector, then you do not need this function.
Hi am unable to understand few points regarding BQ25570EVM evaluation board.
These are few doubts I have in powering a wireless node with BQ25570EVM evaluation board.
Thank you.
1. OK_HYST is the rising VSTOR voltage at which the VBAT_OK_signal will go high. OK_PROG is the falling VSTOR voltage at which the VBAT_OK signal will go low. The intent was for the VBAT_OK to tell your system (and/or the internal buck regulator via the VOUT_EN pin) to turn on and off. The assumption is that you only want operation when the battery is within the voltage range set by OK_HYST down to OK__PROG.
2. Yes.
3. You use the external resistor divider with midpoint connected to the VOUT_SET to set VOUT. You can use the spreadsheet at this link to help. http://www.ti.com/lit/zip/sluc484
4. You must change the resistor values on the EVM board in order to get different values.
5. You change the resistors with midpoint connected to VBAT_OV to change the overvoltage set point.
6. You can use the spreadsheet at the link above to help size the VOUT resistors.
7. As long as the open circuit voltage of your harvester connected the IC's VIN_DC pin is less than 5.5, you should not need any protection.
Also, please read the datasheet Layout section carefully as it warns of solder flux causing parasitic resistors if the boards are not carefully cleaned after soldering.
Thank you very much,But still these are the doubts still remain:
1. VBAT_UV provides overdischarge protection and will open the FET between VBAT and VSTOR so that the system connected to VSTOR cannot pull the battery below the VBAT_UV threshold. The VBAT_OK signal is simply a comparator that signals when the VSTOR=VBAT voltage (where VBAT_UV threshold < OK_PROG threshold) is within the user defined range.
2. VBAT_OK = hi when the voltage at VSTOR is between OK_HYST and OK_PROG.
3. & 4. See 1 and 2 above.
5. You will need a soldering iron and some solder to replace the resistors.
6. The IC needs at least 100uF of equivalent capacitance on VBAT to operate. If you attach a battery with at least that much capacitance, you do not need the 100uF capacitor and can remove it.
7. CBYP filters out high frequency switching noise that could interfere with some of the internal circuits.
8. The buck converter will regulate the output voltage to the VOUT_SET point and provide current up to its peak current limit. If more current is required by the load, the buck converter will simply operate at its peak current limit, turning into a constant current source and the voltage at VOUT will start to drop.
9. No. The resistor divider allows you to scale the output voltage from 1.3V to its maximum of VBAT_OV - 0.2V. Any adjustable output voltage regulating IC uses a resistor divider to divide down the sensed output voltage by the top resistor to the reference voltage, in this case VBIAS=1.21V.
Hi,