Basically I'm designing an thermal energy harvesting setup with supercaps. I've done a bunch of different configs, but lets say for this I'm using two 1F 2.7V in series, so that I get 0.5F 5.4V.
I currently am using two TI evms, and they work great. I have the bq25505eevm that collects the energy from peltiers and the TPS61202EVM that boosts/regulates the collected power from the supercaps to a constant 5V.
However. I don't want the 61202 to turn on and start draining the supercaps until the the caps are at a certain voltage. say 4.7 or 5V or somevalue. and then I want the 61202 to turn off when the caps reach an output voltage of 1.3V or something. Honestly, the turn off point doesn't matter because eventually the 61202 doesn't output enough voltage anyways.
The problem is the 61202 turns on when the supercap output voltage is at 0.5V. But then what happens is that I can never get enough voltage into the caps to do anything useful....
Any suggestions would be amazing.
Thanks!
Aaron Visser