I am using a BQ24735 and I have it successfully charging a 3 cell lipo pack to 12.6V.
The DC supply to the IC is currently sitting at 19.2V. When the supply is connected the System Voltage is sitting at 19.2V . When the supply is disconnected, the system Voltage is the battery voltage of 12.6V.
I would like to have the system voltage constantly at or somewhere near 12.6V. But if I decrease the supply voltage below around 18V the system voltage reverts to the battery voltage, even though the supply is still connected. Can the Supply voltage be somewhere near the battery fully charged voltage of 12.6V ? If so, how is this achieved?
Thanks
A
Thanks
Andrew