I am developing a design for a Lipo Charger for an embedded device and I am using a BQ24735 EVM to get the design started.
During testing I used a digital load to discharge the battery at 500mA and I was expecting the System voltage to be shut off once the Battery voltage passed below 8.943V. Which is 70.97% of the charge voltage (12.6V)
I discovered that the Battery Voltage went past this number and kept on dropping until I terminated the test.
Am I correct in saying this device does not support low battery voltage cutout? Given the inherent danger with lipos being over discharged, how might I implement a low voltage cutout on the battery?
Any suggestions appreciated
A