Hello I have board with schematics mentioned below. I'm using 2000mAh battery connected to bard and I'm charging the battery via USB or AC input. Via AC input the charging is done OK, but with charging via USB input not. Also the voltage on the output goeas above 4.4V I repeated measurement few times with the same result (AC charging is working, USB not). USB charging gives every time different results, but every time it does not charge correctly (also battery full does not lit up). Can someone help me with it?
AC input charging
red: output of BQ chip
blue: battery voltage
green 3.3V board output
USB charging input