Hi everyone!
I'm really a non-expert in battery-management, so I will ask for help before designing something (it is hobby only, no consumer product) that will take me time and then will not function properly.
What I want to do: I got a lamp that is normally connected to a small wall-plug adaptor. It contains a hand full of LEDs driven by a TPS61161. I want this to be portable to take it out (of course while still illuminating my way) so it needs to be battery powered as well.
The goal is to charge 4 in series connected AA NIMH batteries (2200mAh). And this should be done in less than 15 hours at C/10, that's why I'm looking for something able to kind of "fast-charge" my batteries. Since the battery pack will be replaceable, I do not plan to connect a thermistor. This will limit my maximum charge current. Now the first question for you experts: What is a suitable charge-current without sensing the temperature? I was thinking about something like 500mA which results in ~C/4. Possible? Could go lower, but the batteries should be charged over night (~8hrs).
Furthermore the PMIC should detect a full battery and then go over to trickle charge mode to not damage the cells. The wall-plug adapter is connected all the time - the power will never be removed. If the wall-plug adapter is connected, the device should be powered by it, switching over to the batteries if not. I do not plan to build something rocket-science-like, but it should do it's job well.
I'm familiar to electronics - only well done battery charging is new to me. Of course I was searching the internet for different solutions and I had a detailed look at the TI components browser.
An IC that seems to fit into my application is the BQ2002 series in combination with a LM317. Second question: What do you think - is that still a good solution for charging batteries? It has -dV and peak voltage detection termination. It looks simple and I found this application note:
http://www.ti.com/lit/ug/sluu007b/sluu007b.pdf
But there isn't really much better stuff concerning this IC. Other threads like this one:
http://www.eevblog.com/forum/beginners/battery-charger/
haven't pictures in it anymore.
Third question: What are all those different types of BQ2002/F/..... I can't see the differences at first sight.
I link the schematic in:
This is quite clear to me, only a few things: Why do I need Q2? Thought the BQ has an integrated open-collector at CC, too. What is R15 for? Maybe simple, but I just don't get it at the moment. First I was wondering about the voltage regulation for the circuit, but then had a look at D1 which is a zener (wrong symbol), which then makes sense.
Could you provide me any help?
Thanks, Dennis