This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24167's battery detection problem.

Other Parts Discussed in Thread: BQ24167

Hi all, 

I am facing strange problem with BQ24167. It's battery detection loop is getting un-stabilized. I have attached waveform for SYS voltage. It is constantly moving from 4.3V (no-battery) to 3.85 V. Surprisingly, the power good and charging signals are always low and not toggling.

When the charging source is removed the battey voltage is 3.75V and the system voltage is also 3.75V. What could be the problem ? Please let me know if any more details are required

.