I am looking for Battery charger IC which can charge 4s cell Li-Po Battery with up to 3A.
I saw TI product bq24170 & bq24172 and it can support 2~4cell battery in the webpage.
From the datasheet, I understood bq24170 can only 1~3-cell.
And as I know output voltage of bq24172 is adjustable and I thought It can be support 4-cell with adjustable output voltage.
To support 4-cell, the output voltage must at least 16.8V.
But the recommanded output voltage is just to 13.5V and there is no mention about 4cell.
So I wonder,
1. Can bq24172 support 4s cell Li-Po Battery?
2. If it can support, is it right that the value of R2 and R1 to FB port is 698K & 100K?
3. We will use 12V/5A adaptor, but I hope to use recommended DC adaptor for power efficiency.
Regards,
Mykim.