Hi,
In BQ24075, when VIN is below VBAT + VIN(DT), Q1 FET connected between IN and OUT pins is off, CHG/ and PGOOD/ are high. Q2 FET that connects BAT to OUT is ON.
So Vout for the systems will be 3.7V if we are using a Li Ion battery. (Supplement Mode)
As per the datasheet, Vin> VOUT +VDO, the VOUT(reg) is 5.5V and VBAT(reg) is 4.2V. (Normal Mode)
When Vin is less than VOUT but greater than VBAT, how will the output of the system vary (DPPM Mode) ?
Vout will be clamped at 4.3 V ?
And any input voltage below 4.3V will shift it to supplement mode, if not then how will it vary?
Regards,
Apurwa