What is the expected behavior of bq24073 if the battery is absent and the input supply is around 4.4-4.5V?
I notice oscillation on the output while sweeping input from 3V to 6V and hitting that range. It then goes away as voltage increases. It also goes away if battery is connected. Is that expected or am I missing something here? Thanks!