I am using a circuit based on the one in the BQ2000T data sheet (Figure 11 page 13 rev D). It is charging a 3 cell NiMH battery at about 1 amp. It worked fine when charging a 1.8Ah battery, but now we are switching to a higher capacity battery of 2.4Ah, and I am getting some problems.
What I am seeing is that the batteries are getting a lot hotter when being charged. I have changed the resistor divider on the TS input to allow a higher temperature on the thermistor, but I am still not getting a consistent termination. With some batteries the charger will terminate on high temperature cut-off rather than delta T.
My question is can I reduce the charging current to reduce the heating in the batteries, while still detecting the temperature rise at end of charge? What is the minimum charge rate for reliable delta T detection?
Thanks,
Phil