Dear all,
I am using BQ24195 and use it to charge my battery. A USB power source(5V 2A) is plugged in. However, the current it provides is less than the set value. I did the following procedures:
- Write 0x1B to REG01 (Power-On Configuration Register)
- Write 0x36 to REG00 (Input Source Control Register)
- Write 0x8A to REG05 (Charge Termination/Timer Control Register)
- Write 0x00 to REG06 (Thermal Regulation Control Register)
The REG08 is 0x00 and the current I measured is about 90mA. It seems current limit was forced to set to be 100mA and the BQ24195 didn't detect the USB source.
Is there anything wrong? Thanks.