A customer is evaluating the BQ24715 using the EVM and has noticed an audible noise issue. Here is the input from the customer :
So we have been chasing some audible noise coming from the battery charger for a few days now. We are now able to recreate it with EVM feeding our system. if there is a static load the EVM is quite once we attach to our system (dynamic load, mother board with uP) the humming comes back. Any suggestions on ways to mitigate the noise?
Also, the User's Guide for the EVM references a GUI, but there is no S/W to download for the BQ24715EVM. BQStudio does not seem to support this device. Where can the referenced GUI be downloaded?
Thanks for your help!
9/9/15[LE]>also comment about snubber circuit on EVM; will this be helpful in this case?