Without Battery connected, Output voltage of BQ24251 drops when the input voltage is approx. 4.66V. Load current is approx. 800mA.
Datasheet specifies min. operating voltage as 4.35V. I would like to know why the PWM On period is reducing at 4.66V and why the output voltage is dropping.
Also would like to know what happens when the input voltage is less than 4.35V.
Above plot shows voltage at SW pin (Top) and SYS pin (Bottom) When VIN=4.78V
Below plot shows voltage at SW pin (Top) and SYS pin (Bottom) When VIN=4.66V