Hello,
I would like to charge a Lipo of 400 mAh with the BQ25015.
For this Lipo, the recommended max charging current is 400 mA.
If I set the ISET2 to high to get charging current between 400 and 500 mA, is the BQ25015 detecting that it can't go further than 400 mA? or is it the battery that limit the charging current? or is the BQ25015 will charge at 500 mA and my battery will blow up to my face?
If I set ISET2 to low, it will charging at 100 mA, it's too slow.
Thank you for your lightnings