Dear TI,
We are evaluating the bq2589x family (sreceived full bq25890_2 datasheet but still waiting for the datasheet of the bq25895..)
Questions:
In the datasheet SLUSBU7A page 50. REG14 is R/W bits PN[1]/[0] define the device configuration, it these are read/write than basically the chip can be used in both setups, I am correct?
OTG current limiting: does the devices work in constant current mode(with voltage dropped offcourse) if the OTG current is exceeded ? Does it cut of the VUSB OTG voltage if below 3.8V or works normally in constant current mode, regardless of the output voltage?
We have a preliminary version of the bq25895 pdf, based on that the questions are:
bq25895 is it possible to connect PMID boost mode output to VBUS to use one USB input and OTG connector?
Diff. between bq25890/2 and bq25895 is PMID output and JEITA/Hot-Cold charging scheme, or also some other major feature?
11.4.15.1 Over-Current Protection
(bq25890/bq25892)
The charger device closely monitors the RBFET (Q1), HSFET (Q2), and LSFET (Q3) current to ensure
safe boost ode
operation. During over-current condition when output current exceed (IRBFET_OCP) the device will operate
in hiccup mode ...
(bq25895)
This feature is not available for power bank spin - what does this mean??
Br,
Laszlo