Hey, I am trying to use Bq2057C Battery charger to charge single cell Li-ion Battery. I have rigged up the circuit similar to circuit shown in the DV2057 (page 3). I have set the Rsns as 0.2 ohm. And the same PNP transistor (FZT788B). The is battery is charging but at 210mA. I found that the the voltage across the Rsns resistor is ~43 mV.
1. Temperature compensation is disabled. Ts is connected to Vcc/2.
2. Vcc is 5V
3. I have not used the auto comp feature.
What is it that I am missing?
Thanks