hi,
i am working with BQ24075, when i am connecting input supply (5v dc) to pin no. 13 of BQ, my circuit is working fine. when i am connecting battery to BQ 24075, then also is works fine, if there is no USB supply.
But when i connects both battery and external 5v supply, my BQ is getting hot very quickly, i thought it may be because of complete discharged battery. but when i connected a fully charged battery, then also it is gettinh hot.
the circuit i have implemented is attached below.
i am not using POGGD and CHG pin, and i have connected 10kohm resistor on TS Pin, as i havin only two pin on Li-ion battery.
i havev connected 4.12k on SYSOFF pin, i also connected SYSOFF to ground to other PCB, then also BQ is heating. all other parts and value are same as attached in the circuit.
Please provide me some solution, as i am almost on production stage and facing this issue now. my system required current is 2amp.