I want to use the BQ25120 or BQ25121 in a system with a CC2640. I am trying to work out if I need a pull up on the CD line so that the device will power up correctly. As I understand it from the datasheet if there is no VIN and CD is low (default state due to pull down) and the processor pin is tristate before its programmed then the device will be in Hi-Z state. The data sheet says that in Hi-Z state "the SYS output is powered by BAT". Does that mean that the DC/DC converter is working and the SYS output will be regulated to 1.8V (or 2.5V if using the 25121)?