Hi,
Now we are using the BQ25505EVM to do some evaluating,we meet some problems as below:
1.The input is solar panel;
2.Connecting 16K resistor and 2000uF capacitor in parallel to the VSTOR pin as system load;
3.Connecting 10F supercapacitor to the VBAT_SEC for charging.
We measuring the VSTOR pin ,the output voltage is only 1.8V.This is not suitable for application.
How to get a normal output voltage from VSTOR pin?
Thanks!