Hello,
I'm designing a system with a BQ24773 and a BQ34Z-1xx, and for initial prototypes I'm using the EVMs for both ICs and a EV2400 for communication.Currently if I connect both devices to the EV2400, the BQ34x is detected on bqStudio and it's interface shows up. To select the BQ24773 the interface it needs to be the only device, and when opening bqStudio it needs to be manually selected.
Is it possible to utilize the bqStudio software with both devices at the same time ( connecting them both to the I2C bus)? On our final design both devices will be on the same I2C bus.