Hi TI Experts,
Our side is planning to use the BQ24230 as the battery charger IC.
Battery: Single Cell Li-Po
Input Voltage: 24V
We choose the BQ24230 due to the Power Path Management.
According to the datasheet, if the adapter is present, the battery charger IC will give priority to the adapter to power the load.
When the input source is disconnected, only then it will switch to battery for power the load.
This is my understanding, Is that correct?
In addition, can the BQ24230 allow the battery to power the load during the present of adapter?
Is there any hardware configuration need to be done?
If not, is there any TI's battery charger that has this feature?
Because we may need this feature on the application.
Please advice.
Thanks,
Br,
Teach Me