Hi,
When using the BQ25120 communicate with the host in I2C mode,can we disable the watchdog timer?
If it is possible,how to set the register?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
When using the BQ25120 communicate with the host in I2C mode,can we disable the watchdog timer?
If it is possible,how to set the register?
Thanks!
Hi,
I know this post is one month old but Jerry have you got any idea how to disable the watchdog timer?
From my device, what I did was that, when only powering the device by a battery, I put the device in active mode (by CD pin), change the SYS output voltage and put the device back in Hi_Z mode. In this case, the watchdog timer did not reset the registers and the SYS voltage did not change. If I keep the device in active mode, then the timer resets the registers.
Hope this helps.
-Vala
Vala,
There is not a way to disable watchdog timer on the BQ25120. Polling the device every 30s or so will make sure that the watchdog is not reset.
if you are using the BQStudio- i would recommend to use the Autoread function.
We are considering a watchdog disable spin of the BQ25120 in the future which is an OTP setting. (one time programmmable- similar to firmware)
regards,
gautham