Hi,
1. I am using the BQ24295 GUI, and when I check the USB OTG to 1.3A, the REG01 bit 0 changes to 1. However, looking at the datasheet, it says that REG01 bit 0 is Reserved (set to 1). Is the GUI not up to date, or is this a typo on the datasheet?
2. Is there a specific purpose for the FORCE_20PCT bit besides an easy 1 bit change to the charge current? When would one use that bit?
Thanks,
Josh