Hi All,
I'm going to use bq24296. Main source will be input power source and when the one drops, a battery must help to supply a load with the necessary current.
1. As I understand if battery is being charged, internal BATFET is on. If input voltage source is on the limit, Vsys will drop to Vbat, then battery will automatically help to supply the load(supplement mode).
2. However, if VSYS_MAX = 3.8V and battery charge has finished (BATFET is off) what voltage will be on the Vsys? I guess Vsys will be VSYS_MAX or a bit more.
3. Then Conditions are the same:
- VSYS_MAX = 3.8V
- BATFET is Off
How fast BATFET will open and howVsys will drop if more Isys current is needed and bq24296 enters supplement mode?
I see a parameter in the datasheet VSYS_BAT: SYS/BAT comparator, VSYS falling, 70 mV. Is this the value when BATFET will turn on?
Please help me to understand a logic of the IC better.