Hi,
We are using BQ24192 in our design. The bus voltage is 12Vdc.
We configure our devices in sleep mode by turning off the charging and other peripherals supplies.
When battery is connected to the device , the device draws 15-20 mA more current at the VBUS +12V input (90mA), whereas if we disconnect or remove the battery , the current reduces by 15-20mA at the input (70mA).
Please suggest the possible root cause of this issue.
Regards,
Rajkumar Jain