Hello.
When the battery is not fully discharged, BQ21040 operates well.
But, When the battery is fully discharged and the battery protection module of battery detects over discharging, I can not charge the battery.
The OUT pin of BQ21040 is around 0.4V only. There is no battery detection waveform on OUT pin.
I used 1K ohm between Iset and GND. and 10K ohm between TS and GND. Battery is always attached.
Thank you.