Hello, my name is Jose, I would like to know how I can get max current in BQ24296MEVM-655, I have read the datasheet of BQ24296M. In this datasheet in pag 24, I can read the next text: "if ILIM pin is short, the input current limit is set by the register."
I understand that to get max current I have to write 3 Amps in register of charger and pin ILIM I have connect to GND. I would like to know if I am right.
I have now connected BQ24296MEVM-655 to PC with EV2400, the charger to a battery and to a power supply. This power supply can give up to 5 amps. I have set a voltage of 5V in this power supply. And the registers have the following configuration:
- Reg00: 0x37
- Reg01: 0x1B
- Reg02: 0x9C
- Reg03: 0x10
- Reg04: 0xAE
- Reg05: 0xBC
- Reg06: 0x73
- Reg07: 0x4B
I have set the max current 3 amps, in the register REG00[2-1] I have write 111, and I set PSEL to LOW. But I do not get load 3 amps, I got 1,1 amps max. I Think that this limitation is caused by the potentiometer, the max current above mentioned was get with the potentiometer at max place.
I would like to know how I can get max current in BQ24296MEVM-655,
thanks in advance,
Jose.