We are working on a design using BQ25895 - The scheme is simple. The load is powered by mains when mains in ON. Battery takes over when mains is OFF. We have connected the load to PMID pin.
The load is approx 2A peak, 700mA average. The adapter (5V source) can supply 3A.
We have tested that the load can be supplied by both mains and using battery boost.
However, the battery is not charging in any condition. There are no faults when reading the I2C registers and the input is being detected as USB DCP = 3.25A.
The registers also indicate charge mode enabled (when mains is available) and device is in fast-charge mode. But both the ADC readings and actual readings show charge current a 0.
Please see the attached schematic of our design.
We have tried by bypassing the battery protection circuit (bq29700) also. The result is the same.
--
Please help us resolve the issue.
Thanks and Regards,
Saurabh